SPRAD86 March 2023 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM68A , AM69A
Locate and run the installed tuning tool executable in Windows, <installation folder>\bin\DCC.exe. Choose VPAC3L (AM62A) when prompted for the correct VPAC version. After the tool starts, create a project and enter raw image properties. #GUID-1997A11A-6856-4D0F-BB87-FAD449F01960 shows an example for IMX219 in 1080p streaming mode.
Once a new project is created, raw images can be previewed through the tuning tool. Capture a raw image of the color checker with good lighting condition using the command for camera capturing verification. Select this image file in the tuning tool's "Browse" window and the image should display in the "Preview window". For example, below is an IMX219 raw image at 1920x1080 with 10 bits per pixel, displayed in the tuning tool.
Now that everything is ready, one can proceed to perform tuning, as described in following sections.