SPRADP6A February 2025 – May 2025 AM2612 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
If the JTAG scan-test is successful, then right-click the Target Configuration ccxml file → Launch Selected Configuration.
Figure 5-8 Launch the Target
ConfigurationOnce loaded, right-click on the R5_0 core and click Connect Target in the Debug window.
Figure 5-9 Connect TargetObserve the console output. If the output console is not visible, then select View → Console in Code Composer Studio.
Connecting to the AM26x target automatically loads GEL (General Extension Language) files to the AM26x R5F Core to initialize the AM26x device. This includes configuring device clocks, enabling peripheral clocks, and unlocking control registers.
GEL files can also be manually loaded to the AM26x device. While this is not recommended for initial bring-up, this allows for more customization and bring-up of specific device blocks, rather than the entire set of AM26x peripherals.
Figure 5-10 Open GEL Files
ViewIf no errors are observed in the output console, then JTAG connection to the device is verified.