SPRU514Y August 2001 – June 2022
If the --idiv_support=idiv0 command-line option is used, the compiler generates faster instructions to perform integer division when the division ("/") or modulo ("%") operator or the div() or ldiv() function is used. The faster versions of these built-in operators are used whether or not the
stdlib.h
header file is included.
The following table shows which intrinsics are used to perform integer operations using the division ("/") and modulo ("%") operators.
Types Operated Upon | Equivalent Intrinsic Call |
---|---|
int / int | __traditional_div_i16byi16(int, int).quot |
int % int | __traditional_div_i16byi16(int, int).rem |
unsigned int / unsigned int | __traditional_div_u16byu16(unsigned int, unsigned int).quot |
unsigned int % unsigned int | __traditional_div_u16byu16(unsigned int, unsigned int).rem |
long / long | __traditional_div_i32byi32(long, long).quot |
long % long | __traditional_div_i32byi32(long, long).rem |
unsigned long / unsigned long | __traditional_div_u32byu32(unsigned long, unsigned long).quot |
unsigned long % unsigned long | __traditional_div_u32byu32(unsigned long, unsigned long).rem |
long long / long long | __traditional_div_i64byi64(long long, long long).quot |
long long % long long | __traditional_div_i64byi64(long long, long long).rem |
unsigned long long / unsigned long long | __traditional_div_u64byu64(unsigned long long, unsigned long long).quot |
unsigned long long % unsigned long long | __traditional_div_u64byu64(unsigned long long, unsigned long long).rem |
Intrinsics that allow you to more exactly specify the operation to be performed are listed in Section 8.7.4.
In C, when the operands of integer division or modulo operations have different types, the compiler automatically performs "integral promotion" (also called implicit type conversion). That is, the compiler inserts an implicit cast to convert to a common type, and then performs the operation in that type.
The intrinsic that is performed may be different than the one expected based on the types being divided. For example:
long dividend_i32, quotient_i32;
unsigned long divisor_u32, quotient_u32;
int divisor_i16;
/* uses __traditional_div_u32byu32, not __traditional_div_i32byu32 */
quotient_u32 = dividend_i32 / divisor_u32;
/* uses __traditional_div_i32byi32, not __traditional_div_i32byi16 */
quotient_i32 = dividend_i32 / divisor_i16;
Because integral promotion can be confusing, it is often best to avoid the issue by making sure the operand types agree, possibly by using a cast operator. For more about integral promotion, see How to Write Multiplies Correctly in C Code (SPRA683).