SPRU514Y August 2001 – June 2022
The post-link optimizer is not part of the normal development flow. Figure 6-1 shows the flow including the post-link optimizer; this flow occurs only when you use the compiler and the -plink option.
As the flow shows, the absolute lister (abs2000) is also part of the post-link optimizing process. The absolute lister outputs the absolute addresses of all globally defined symbols and COFF sections. The post-link optimizer takes .abs files as input and uses these addresses to perform optimizations. The output is a .pl file, which is an optimized version of the original .asm file. The flow then reruns the assembler and linker to produce a final output file.
The described flow is supported only when you use the compiler (cl2000) and the -plink option. If you use a batch file to invoke each tool individually, you must adapt the flow to use the compiler instead. In addition, you must use the --output_file option to specify an output file name when using the -plink option. See Section 6.9 for more details.
For example, replace these lines:
cl2000 file1.asm file1.c.obj
cl2000 file2.asm file2.c.obj
cl2000 --run_linker file1.c.obj file2.c.obj lnk.cmd --output_file=prog.out
with this line:
cl2000 file1.asm file2.asm --run_linker lnk.cmd --output_file=prog.out -plink
The advice_only mode is the only post-link optimization support provided for FPU and VCU targets.