SPRU514Y August 2001 – June 2022
The linker assumes you are using the C and C++ conventions if either the --rom_model or --ram_model linker option is specified, or if at least one C/C++ file to compile is listed on the command line. See Section 5.4.5 for details about using the --rom_model and --ram_model options.
If the linker assumes you are using the C and C++ conventions and the entry point for the program (normally c_int00) is not resolved by any specified object file or library, the linker attempts to automatically include the most compatible run-time-support library for your program. The run-time-support library chosen by the compiler is searched after any other libraries specified with the --library option on the command line or in the linker command file. If libc.a is explicitly used, the appropriate run-time-support library is included in the search order where libc.a is specified.
You can disable the automatic selection of a run-time-support library by using the --disable_auto_rts option.
If the --issue_remarks option is specified before the --run_linker option during the linker, a remark is generated indicating which run-time support library was linked in. If a different run-time-support library is desired than the one reported by --issue_remarks, you must specify the name of the desired run-time-support library using the --library option and in your linker command files when necessary.