A function (parent function) performs the
following tasks when it calls another function (child function).
- Any registers whose values are not
necessarily preserved by the function being called (registers that are not save-on-entry
(SOE) registers), but will be needed after the function returns are saved on the
stack.
- If the called function returns a
structure, the calling function allocates the space for the structure and pass the address
of that space to the called function as the first argument.
- Arguments passed
to the called function are placed in registers and, when necessary, placed on the stack.
Arguments are placed in registers using the following scheme:
- If the target is FPU and there are
any 32-bit float arguments, the first four float arguments are placed in registers
R0H-R3H.
- If there are any 64-bit floating
point arguments (long doubles), they are passed by reference.
- If there are any 64-bit integer arguments (long long), the first is
placed in ACC and P (ACC holds the upper 32 bits and P holds the lower 32 bits). All
other 64-bit integer arguments are placed on the stack in reverse order.
If the P register is used for argument passing, then
prolog/epilog abstraction is disabled for that function. See Section 4.14 for more information on abstraction.
- If there are any 32-bit arguments
(longs or floats), the first is placed in the 32-bit ACC (AH/AL). All other 32-bit
arguments are placed on the stack in reverse order.
func1(long a, long long b, int c, int* d);
stack ACC/P XAR5, XAR4
- Pointer arguments are placed in XAR4
and XAR5. All other pointers are placed on the stack.
- Remaining 16-bit arguments are placed
in the order AL, AH, XAR4, XAR5 if they are available.
- Any remaining arguments not placed in
registers are pushed on the stack in reverse order. That is, the leftmost argument that is
placed on the stack is pushed on the stack last. All 32-bit arguments are aligned to even
addresses on the stack.
A structure
argument is passed as the address of the structure. The called function must make a
local copy.
For a function declared
with an ellipsis, indicating that it is called with varying numbers of arguments, the
convention is slightly modified. The last explicitly declared argument is passed on the
stack so that its stack address can act as a reference for accessing the undeclared
arguments.
- The stack pointer (SP) must be
even-aligned by the parent function prior to making a call to the child function. This is
done by incrementing the stack pointer by 1, if necessary. If needed, the coder should
increment the SP before making the call. These function call examples show where arguments
are
placed:
func1 (int a, int b. long c)
XAR4 XAR5 AH/AL
func1 (long a, int b, long c) ;
AH/AL XAR4 stack
vararg (int a, int b, int c, ...)
AL AH stack
- The caller calls the function using the
LCR instruction. The RPC register value is pushed on the stack. The return address is then
stored in the RPC register.
- The stack is aligned at function
boundary.