SPRU514Y August 2001 – June 2022
If the compiler tools are to be installed in shared or read-only directory, mklib cannot build the standard libraries at link time; the libraries must be built before the library directory is made shared or read-only.
At installation time, the installing user must build all of the libraries which will be used by any user. To build all possible libraries, change the working directory to be the compiler RTS library directory 'lib' and invoke the mklib executable there:
mklib --all
Some targets have many libraries, so this step can take a long time. To build a subset of the libraries, invoke mklib individually for each desired library.