See
the following resources for further information
about the TI Code Generation Tools:
You
can use the following documents to supplement this
user's guide:
SPRAAB5
The Impact of DWARF on TI Object
Files.
Describes the Texas Instruments extensions to the
DWARF specification.
SPRU513
TMS320C28x Assembly Language Tools
User's Guide describes the assembly
language tools (assembler and other tools used to
develop assembly language code), assembler
directives, macros, common object file format, and
symbolic debugging directives for the TMS320C28x
device.
SPRU430
TMS320C28x DSP CPU and Instruction Set
Reference Guide describes the central
processing unit (CPU) and the assembly language
instructions of the TMS320C28x fixed-point digital
signal processors (DSPs). It also describes
emulation features available on these DSPs.
SPRU566
TMS320x28xx, 28xxx Peripheral Reference
Guide describes the peripheral reference
guides of the 28x digital signal processors
(DSPs).
https://www.ti.com/lit/pdf/SPRUHS1
TMS320C28x Extended Instruction Sets
Technical Reference Manual describes the
architecture, pipeline, and instruction sets of
the TMU, VCRC, VCU-II, FPU32, and FPU64
accelerators.
SPRAC71
TMS320C28x Embedded Application Binary
Interface (EABI) Application Report.
Provides a specification for the ELF-based
Embedded Application Binary Interface (EABI) for
the TMS320C28x family of processors from Texas
Instruments. The EABI defines the low-level
interface between programs, program components,
and the execution environment, including the
operating system if one is present.
SPRUEX3
TI SYS/BIOS Real-time Operating System
User's Guide. SYS/BIOS gives application
developers the ability to develop embedded
real-time software. SYS/BIOS is a scalable
real-time kernel. It is designed to be used by
applications that require real-time scheduling and
synchronization or real-time instrumentation.
SYS/BIOS provides preemptive multithreading,
hardware abstraction, real-time analysis, and
configuration tools.