SPRUHM8K December 2013 – May 2024 F28377D-SEP , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
In IDLE mode, the watchdog interrupt (WDINT) signal can generate an interrupt to the CPU to take the CPU out of IDLE mode. As with any other peripheral, the watchdog interrupt triggers a WAKEINT interrupt in the PIE during IDLE mode. User software must determine which peripheral caused the interrupt.
In STANDBY mode, all of the clocks to the peripherals are turned off within the CPU subsystem. The only peripheral that remains functional is the watchdog since the watchdog module runs off the oscillator clock (OSCCLK). The WDINT signal is applied to the Low Power Modes (LPM) block so that the signal can be used to wake the CPU from STANDBY low-power mode. This feature is enabled by setting LPMCR.WDINTE = 1. See Section 3.10 for details.
Note: If the watchdog interrupt is used to wake-up from an IDLE or STANDBY low-power mode condition, software must make sure that the WDINT signal goes back high before attempting to reenter the IDLE or STANDBY mode. The WDINT signal is held low for 512 INTOSC1 cycles when the watchdog interrupt is generated. The current state of WDINT can be determined by reading the watchdog interrupt status bit (WDINTS) bit in the SCSR register. WDINTS follows the state of WDINT by two SYSCLKOUT cycles.
In HALT mode, the internal oscillators and CPU1 watchdog are kept active if the user sets CLKSRCCTL1.WDHALTI = 1. A watchdog reset can wake the system from HALT mode, but a watchdog interrupt cannot.