SPRUHM8K December 2013 – May 2024 F28377D-SEP , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
On this device, uPP only supports an 8-bit interface; hence, no data packing is performed. In this case, make the appropriate connection externally, if needed. For example, if a 4-bit ADC is used, then tie the upper 4-bits of the uPP data inputs to 0 or 1, as needed. If external FPGA is connected, then make sure that 8-bit data (or appropriate tie-offs) is driven out from the FPGA. By default, uPP supports little-endian data format but to support the data format of one of the TI devices (CC1260), a configuration bit is provided to select 16-bit big-endian mode also.
Figure 24-15 and Figure 24-16 describe how data goes out and comes in based on these modes.
Figure 24-15 uPP Tx Data Pattern in
Non-Interleaved Mode
Figure 24-16 uPP Rx Data Pattern in
Non-Interleaved Mode