SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
RAM blocks that are accessible from the CPU and DMA are called global shared RAMs (GSx RAMs).
Table 3-12 shows the features of the GSx RAM.
| CPU1 | CPU1 | CPU1 | CPU1.DMA | CPU1.DMA |
|---|---|---|---|---|
| Fetch | Read | Write | Read | Write |
| Yes | Yes | Yes | Yes | Yes |
Like other shared RAM, these RAMs also have a different levels of access protection which can be enabled or disabled by configuring specific bits in the GSxACCPROT registers.
Master select and access protection configuration for each GSx RAM block can be individually locked by the user to prevent further update to these bit fields. The user can also choose to permanently lock the configuration to individual bit fields by setting the specific bit fields in the GSxCOMMIT register (refer to the register description for more details). Once configuration is committed for a particular GSx RAM block, the configuration cannot be changed further until CPU1.SYSRS is issued.