SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
When the rule engine is processing a packet, it stored a snapshot of latest 32 octets in an internal buffer. This buffer allows evaluation of expressions on packet octets even after the packet octets have gone by on the external receive VBUSP network interface.
At the start of packet, the first eight octets received are loaded into the first eight locations of the packet buffer. When the next eight octets arrive, these are loaded into the first eight locations and the existing octets are moved to the following eight locations. This process is continued until the packet buffer is full. When packet buffer is full and additional octets arrive, the oldest eight octets are shifted out and are no longer available to the rule engine. Thus, the packet buffer provides a snapshot of most recent octets received.
When the rule engine encounters instructions that reference packet octets which have not yet been received then the rule engine stalls until the required octets are available. Similarly, instructions which require octets that have already been shifted out of the packet buffer will cause rule engine to stall. And since these octets will never be available, the rule engine will not execute any further instructions for the current packet. It will return to the first instruction when the packet ends.
Figure 24-205 Packet Octets as Stored in the Packet BufferThe contents of a packet, when used as one or more operands in an instruction, are always fetched from the packet buffer. The Base registers (B0-B4) in conjunction with an offset and bits are used to specify which octets are to be used as operands.