SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
An additional MMU provides address translation for the accesses done from the IPUx subsystem to the L3_MAIN interconnect. The main characteristics of this MMU are:
The configuration of the MMU can be done from one of the Cortex-M4 cores or from the L3_MAIN interconnect slave port. The accesses done to configure the MMU cannot be part of a burst access.
For more information about the IPUx_MMU, see Chapter 20, Memory Management Units.