SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
The enhanced direct memory access module, also called EDMA, performs high-performance data transfers between two slave points, memories and peripheral devices without microprocessor unit (MPU) or digital signal processor (DSP) support during transfer. EDMA transfer is programmed through a logical EDMA channel, which allows the transfer to be optimally tailored to the requirements of the application.
The EDMA can also perform transfers between external memories and between Device subsystems internal memories, with some performance loss caused by resource sharing between the read and write ports.
EDMA controller is based on two major principal blocks:
The TPCC is a high flexible Channel Controller. It serves as an user interface and an event interface for the EDMA controller. The EDMA_TPCC serves to prioritize incoming software requests or events from peripherals and submits transfer requests (TRs) to the transfer controller.
The TPTC performs read and write transfers by EDMA ports to the slave peripherals as programmed in the "Active" and "Pending" set of the registers. The transfer controllers are responsible for data movement and issue read/write commands to the source and destination addresses that are programmed for a given transfer in the EDMA_TPCC.
The SoC integrates the following EDMA instances:
Each of these EDMA modules consists of:
All EDMA modules in the SoC are functionally identical. Note that some of the configuration parameters may be different for the various EDMA instances (see Section 16.2.1.3, EDMA Controllers Configuration).
This chapter is mostly focused on describing the system-level EDMA module (in terms of configuration and integration in the SoC). For details on DSPx_EDMA / EVEx_EDMA integration, see their respective chapters.
Figure 16-12 shows an overview of the EDMA module.
Figure 16-12 EDMA module OverviewThe device CPUs can configure the EDMA controller blocks through the L3_MAIN interconnect.