SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
Similarly, the receive data ready flag - RDATA in the MCASP_RXSTAT register reflects the data ready status of XRBUFn buffers for all of the active slot receiving serializers. The RDATA flag is set whenever data is transferred from a receiving serializer shift register XRSRn to its corresponding XRBUFn data buffer. Thus, the RDATA bit indicates the global event that some of the receivers data buffer - RXBUFn already contains received data (i.e. a buffer is full) and is ready to transfer it to the host (MPU/DSP). The receive data ready event is individually indicated per serializer in its corresponding control register MCASP_XRSRCTLn [5] RRDY status bit. When this bit is set to 0b1, it notifies to host that this serializer Rx buffer must be serviced (read). When MCASP_RXBUFn is read from the host, the MCASP_XRSRCTLn [5] RRDY is deasserted to 0b0. As RDATA global flag is an OR-event of all active serializers RRDY flags, it indicates to software the moment, when read service operation has to be initiated by the McASP host (RDATA=0b1). The RRDY flags have to be sequentially scanned by user software to determine which serializer MCASP_RXBUFn register has to be currently read. Once all requested MCASP_RXBUFn are read, the serializers control RRDY flags are cleared to 0b0. As a consequence, RDATA flag is deasserted to 0b0, to indicate to SW that read operation is completed for all serializers.
The global RDATA flag can be cleared when the MCASP_RXSTAT[5] RDATA bit is written to 0b1, or once MCASP_RXBUFn registers of all the serializers, that have previously raised their RRDY flags, are read by the host.
Whenever RDATA is set, the AREVT event is automatically generated on MCASPi_DREQ_RX line (if enabled in the MCASP_REVTCTL register) to notify the DMA of the MCASP_RXBUFn full status. An interrupt - MCASPi_IRQ_AREVT can be also generated if the RDATA interrupt is enabled in the MCASP_EVTCTLR register (for details, see Section 24.6.4.12.1, Receive Data Ready Interrupt).
Figure 24-129 shows the timing details of when AREVT event is generated at the McASP boundary. In this example, as soon as the last bit (bit A0) of Word A is received, the McASP sets the RDATA flag and generates an AREVT event. However, it takes up to five McASP interface clocks (AREVT Latency) before AREVT is active at the McASP boundary. Upon AREVT, the CPU can begin servicing the McASP by reading Word A from the MCASP_RXBUFn (service time). The CPU must read Word A from the MCASP_RXBUFn register no later than the setup time required by the McASP (Setup Time).
The maximum service time (see Figure 24-129) can be calculated as:
Service Time = Time Slot - AREVT Latency - Setup Time
Figure 24-129 CPU Service Time Upon Receive Event (AREVT)