SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
To generate high-frequency clocks, the device supports multiple on-chip DPLLs controlled directly by the PRCM module. They are of two types: type A and type B DPLLs.
The following DPLLs belong to type A:
The following DPLLs belong to type B:
All DPLLs (type A and type B) support the features described in the following sections, unless otherwise identified.
This chapter discusses only the DPLLs that are directly controlled by the PRCM module. The other DPLLs embedded in and managed by other subsystems are described in their respective subsystems.