SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
When a protection violation occurs, an interrupt is send to the INTCs (if enabled). An in-band error is sent back to L3 IA and an out-of-band error can also be logged in the CONTROL.CONTROL_SEC_ERR_STATUS register in the SCM. These out-of-band errors are enabled and disabled at the L4 IA level by setting the L4_IA_AGENT_CONTROL_L[31][30] PROT_ERROR_SECONDARY_REP or PROT_ERROR_PRIMARY_REP bit to 1 for debug and application mode, respectively.
At the control module level, two logging registers are used, depending on the mode:
Figure 14-14 shows the global protection error reporting to the control module.
Figure 14-14 Protection Violation Out-of-Band Error Reporting