SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
A Send Interrupt descriptor will cause the VPDMA to generate an interrupt on the list manager controlled interrupts as specified by the Source Field. The list will not stall on this descriptor. For example, if source is 0 then control_descriptor_int0 will fire. If source is 12, then control_descriptor_int12 will fire. For more information ot VPDMA interrupt events, see Section 9.4.8.7, VPDMA Interrupts.
| Bits | Name | Description |
|---|---|---|
| 31:27 | Packet Type | Host Packet Descriptor Type = Ch |
| 26:24 | Reserved | Reserved |
| 23:16 | Source | Specifies the source used for the control event. |
| 15:4 | Reserved | Reserved for future use |
| 3:0 | Control | Control type = 6h |