SPRUIG6L January 2018 – March 2025
All legacy intrinsics defined in
c6x_migration.h
are available for use in C7000 Host Emulation. Their interface is the same as it is with the C7000 compiler.
Section 8 discusses requirements regarding legacy data types and assumptions about their SIMD usage. As a result of those limitations, all legacy data types must be treated as container types. That is, all initialization and interaction with legacy data types must be through intrinsics. Section 8 also contains examples of how to program with legacy data types and intrinsics when using C7000 Host Emulation. The C6000-to-C7000 Migration User's Guide (SPRUIG5) and the
c6x_migration.h
header file should be used as references any time C6000 code is used within a C7000 program.