SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Figure 12-2240 illustrates the counter-compare submodule within the EPWM. Figure 12-2241 shows the basic structure of the counter-compare submodule.
Figure 12-2240 EPWM Counter-Compare SubmoduleCC module features:
The counter-compare submodule takes as input the time-base counter value. This value is continuously compared to the counter-compare A (EPWM_CMPA) and counter-compare B (EPWM_CMPB) registers. When the time-base counter is equal to one of the compare registers, the counter-compare unit generates an appropriate event.