SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The I2C module is a serial bus that supports multiple controller devices. In multicontroller mode, one or more devices can be connected to the same bus and are capable of controlling the bus. Each I2C device on the bus is recognized by a unique address and can operate as either a transmitter or a receiver, depending on the function of the device. In addition to being a transmitter or receiver, a device connected to the I2C bus can also be considered a controller or a peripheral when performing data transfers.
A controller device is the device that initiates the data transfer on a bus and generates the clock signal that permits the transfer. During the transmission, any device addressed by the controller is considered the peripheral.
Data is communicated to devices interfacing to the I2C module using the serial data pin (SDA) and the serial clock pin (SCL) as shown in Figure 13-6. These two wires carry information between the device and the other devices connected to the I2C bus. Both SDA and SCL pins on the device are bidirectional. They must be connected to a positive supply voltage through a pull-up resistor. When the bus is free, both pins are high. The driver of these two pins has an open-drain configuration to perform the wired-AND function.
The device has a special mode that can be entered to ignore a NACK generated from non-compliant I2C devices that are incapable of generating an ACK.
The I2C module consists of the following primary blocks:
In Figure 13-6, the CPU or the DMA writes data for transmission to ICDXR and reads received data from ICDRR. When the I2C module is configured as a transmitter, data written to ICDXR is copied to ICXSR and shifted out one bit at a time. When the I2C module is configured as a receiver, received data is shifted into ICRSR and then copied to ICDRR.
When the I2C function is not needed, the pins may be controlled as general-purpose input/output (GPIO) pins. The I/O structure of each pin includes:
Figure 13-6 Simple I2C Block Diagram