SPRUJ17I March 2022 – August 2025 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The DCC may be programmed to count down one time using single-shot mode. In this mode, the DCC stops operation when:
At the end of one sequence in single-shot mode, the DCC will de-assert the enable value (DCCENA), disabling further counting. At the end of one sequence in single-shot mode, if it is no error that stops counting, then the done status bit is set and a done interrupt is driven. Application must clear the done bit before restarting counts. At the end of a sequence in single-shot mode, if there is an error, then the error status bit will be set. Application must clear the error status bit before starting the next sequence.