SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
This is the DDR50 mode where the eMMC CLK is set to 50 MHz. The data is driven on both the edges of the clock. To emulate the Interface timing, a Hold time is inserted on Transmit data lines by using the Phase shifted TX Clock. The amount of phase shift can be from 1 to 16 Taps. In this mode, the TX Clock Phase shift is being performed by using one of the first 16-taps of the DLL TXCLK Phases. The Phase shifting on the RX path is disabled in this mode.