SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
XIP mode is supported in most FLASH devices. Some of them use signature bits that are sent to the device immediately following the address bytes, other use signature bits and also require a FLASH device configuration register write to enable XIP. For the FLASH devices that must be compliant to the OSPI controller, the following steps can be taken by software to enter XIP mode: