SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
FILE: usb_ex1_dev_serial.c
This example application turns the evaluation kit into a virtual serial port when connected to the USB host system. The application supports the USB Communication Device Class, Abstract Control Model to redirect SCIA traffic to and from the USB host system.
Connect USB cables from your PC to both the mini and microUSB connectors on the controlCARD.Figure out what COM ports your controlCARD is enumerating (typically done using Device Manager in Windows) and open a serial terminal to each of with the settings 115200 Baud 8-N-1. Characters typed in one terminal should be echoed in the other and vice versa.
A driver information (INF) file for use with Windows XP, Windows 7 and Windows 10 can be found in the windows_drivers directory.