SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Resolver to Digital Converter(RDC) in AM263P contains all the signal processing blocks needed to extract the position and velocity using the Sine and Cosine signals generated from an external hardware Resolver. As shown on Figure 7-137and Figure 7-139, there are two identical blocks, termed as RDC Core-0(RDC0) and RDC-Core1(RDC1), on the SOC.
The following sections explain the different signal processing blocks of this RDC sub-system.