SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The mapping between the DMA channel numbers and the PaRAM sets is programmable (see Parameter RAM (PaRAM)). The DMA channel mapping registers EDMA_TPCC_DCHMAPN_m in the EDMA_TPCC provide programmability that allows the DMA channels to be mapped to any of the PaRAM sets in the PaRAM memory map. Figure 11-12 illustrates the use of EDMA_TPCC_DCHMAPN_m. There is one EDMA_TPCC_DCHMAPN_m register per channel.
Figure 11-12 DMA Channel and
QDMA Channel to PaRAM Mapping