A functional block diagram of the PRU-ICSS UART0 is shown in Figure 7-51.
NOTE: The value n indicates the applicable UART where there are multiple instances. For the PRU-ICSS, there is only one instance and all UART signals should reflect this (e.g., UART0_TXD instead of UARTn_TXD).