SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
If conversion timings can be made sure to not overlap by the user, then all the SOCs on all ADCs do not have to be identically configured to achieve performance equivalent to synchronous operation. For example, if the two ADC triggers in a system come from two ePWM sources that are always 180-degrees out-of-phase, then SOC0 can be used for both ADCA and ADCB with different trigger sources and different ACQPS values.
Figure 7-136 Example: Synchronous Equivalent Operation with Non-Overlapping Conversions