SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from the EPWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 7-312. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 7-313.
Figure 7-312 Details of the Counter and
Synchronization Block