SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
The standard Message ID (11-bit ID) filtering flow is shown in Figure 13-173. Section 13.4.1.4.10.5, Standard Message ID Filter Element describes the standard Message ID filter element.
The Remote Transmission Request (RTR) and Extended Identifier (XTD) bits of the received frames are compared against the list of configured filter elements. This is controlled by the following registers:
Figure 13-173 Standard Message ID Filter Path