SPRUJ55D September 2023 – July 2025 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
Figure 13-155 shows the OSPI module block diagram.
Figure 13-155 OSPI Block DiagramThe OSPI module is composed of three main blocks. The first one is the OSPI controller, the second one is the low level SPI protocol controller, and the third one is the integrated PHY.
The OSPI module has the following two target interfaces: