SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
FILE: esm_cpu1_cpu3_multi_c29x1.c
This example demonstrates how to handle fault conditions using ESM and Error Aggregator in a muli-core example (ESM_cpu1_cpu3_multi_c29x1.c).
When using CCS for debugging this Multi-core example, after launching the debug session,
For FLASH configuration, this example is run in FLASH BANKMODE2, where CPU3 has access to FLASH (FRI-2). Refer to the Flash Plugin documentation to know about changing FLASH BANKMODEs and more. Additionally, the CPAx and CDAx RAMs are used for allocating various RAM sections.
External Connections
Watch Variables