SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
Upon an error generated by the LCM module, an error event input is sent to the error signaling module (ESM). The ESM can be configured to take appropriate action that includes error status pin indication, generation of an interrupt or NMI to the CPU. The LCM error can be triggered by any of the following:
To determine the specific cause of the LCM error-induced NMI, the LCM_STATUS register bits can be read. Particularly:
For details on system-level NMIs vector locations and interrupt-handling, see Chapter 6.