FILE: epwm_ex4_digital_compare.c
This example configures ePWM1 as follows
- ePWM1 with DCAEVT1 forcing the ePWM output LOW
- GPIO2 is used as the input to the INPUT XBAR INPUT1
- INPUT1 (from INPUT XBAR) is used as the source for DCAEVT1
- GPIO2's PULL-UP resistor is enabled, in order to test the trip, PULL this pin to GND
External Connections
- GPIO0 EPWM1A
- GPIO1 EPWM1B
- GPIO2 TZ1, pull this pin low to trip the ePWM
Watch Variables