SPRUJA3 November 2024 F29H850TU , F29H859TU-Q1 , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28378D , TMS320F28379D
F29H85x has two dedicated VREFHI pins. One is for both ADCA and ADCB (12-bit/16-bit ADCs) and the other is for ADCC, ADCD, and ADCE (12-bit ADCs). These VREFHI pins should not be tied together but instead be supplied independently to minimize coupling between the different ADC types and modes of operation to achieve optimum performance.
In addition, it is important to keep low inductance connections in the reference path allows the reference driving circuit to remain stable and settled during the conversion phase.