SPRUJB6B November 2024 – May 2025 AM2612
The first criteria that must be selected is whether both EPWM channel A and channel B outputs are required. If both channel A and channel B are required, XCMP registers must be assigned to both CMPA and CMPB. The XCMPn registers loaded to CMPA are used for configuring the A channel through XAQCTLA actions. The XCMPn registers loaded to CMPB are used for configuring the B channel through XAQCTLB actions.
XCMP allocation to CMPA and CMPB is done through XCMPCTL1.XCMPSPLIT. If both channel A and channel B are required in the system, then the XCMPCTL1.XCMPSPLIT must be set. This allows CMPA to use XCMP1-n (where n has a maximum value of 4) while CMPB uses XCMP5-m (where m has a maximum value of 8). If only channel A is needed, then XCMPCTL1.XCMPSPLIT must be cleared, allowing CMPA to use XCMP1-n (where n has a maximum value of 8), which means up to eight edges can be generated on channel A.
XCMPA_ALLOC and XCMPB_ALLOC determines how many of the available XCMPs for each CMPA and CMPB must be used in the ePWM configuration.