SPRUJB6B November 2024 – May 2025 AM2612
The MDIO module will remain idle until enabled by setting the [30] ENABLE bit in the MDIO MDIO_CONTROL_REG register. The MDIO will then continuously poll the link status from within the Generic Status Register of all possible 32 PHY addresses in turn recording the results in the MDIO MDIO_LINK_REG register. Individual PHY's can be enabled or disabled for polling through the associated bit in the MDIO MDIO_POLL_EN_REG register. The MDIO MDIO_LINK_REG and MDIO_ALIVE_REG register bit values are updated on the poll of each PHY. In Normal Mode, the link status of two of the 32 possible PHY addresses can also be determined using the MLINK pin inputs. The bit [7] LINKSEL in the MDIO MDIO_USER_PHY_SEL_REG_0/1 register determines the status input that is used. A change in the link status of the two PHYs being monitored will set the appropriate bit ([1-0] LINKINTRAW) in the MDIO MDIO_LINK_INT_RAW_REG register and the MDIO_LINK_INT_MASKED_REG[1-0] LINKINTMASKED register, if enabled by the [6] LINKINT_ENABLE bit in the MDIO MDIO_USER_PHY_SEL_REG_0/1 register. In State Change Mode, a change in any PHY status will be indicated on the MDIO_LINK_INT_RAW_REG[0] LINKINTRAW interrupt if enabled.
The MDIO MDIO_ALIVE_REG register is updated by the MDIO module if the PHY acknowledged the read of the generic status register. In addition, any PHY register read transactions initiated by the host also cause the MDIO MDIO_ALIVE_REG register to be updated.
At any time, the host can define a transaction for the MDIO module to undertake using the [15-0] DATA, [20-16] PHYADR, [25-21] REGADR, and [30] WRITE fields in a MDIO_USER_ACCESS_REG_0/1 register. When the host sets the [31] GO bit in this register, the MDIO interface module will begin the transaction without any further intervention from the host. Upon completion, the MDIO will clear the [31] GO bit and set the [1-0] USERINTRAW bit field in the MDIO_USER_INT_RAW_REG register corresponding to the MDIO_USER_ACCESS_REG_0/1 register being used. The corresponding bit in the MDIO_USER_INT_MASKED_REG register may also be set depending on the mask setting in the MDIO_USER_INT_MASK_SET_REG and MDIO_USER_INT_MASK_CLEAR_REG registers. A round-robin arbitration scheme is used to schedule transactions which may queued by the host in different MDIO_USER_ACCESS_REG_0/1 registers. The host should check the status of the [31] GO bit in the MDIO_USER_ACCESS_REG_0/1 register before initiating a new transaction to ensure that the previous transaction has completed. The host can use the [29] ACK bit in the MDIO_USER_ACCESS_REG_0/1 register to determine the status of a read transaction.
Software may use the MDIO module to set up the auto-negotiation parameters of each PHY attached to a MAC port, retrieve the negotiation results, and set up the MAC Control register in the corresponding MAC.