SPRUJB6B November 2024 – May 2025 AM2612
The 10-bit addressing format is similar to the 7-bit addressing format, but the controller sends the peripheral address in two separate byte transfers. In the 10-bit addressing format (Figure 13-12), the first byte is 11110b, the two MSBs of the 10-bit peripheral address, and the R/ W bit. The ACK bit is inserted after each byte. The second byte is the remaining 8 bits of the 10-bit peripheral address. The peripheral must send an acknowledgement after each of the two byte transfers. Once the controller has written the second byte to the peripheral, the controller can either write data or use repeated a START condition to change the data direction.
To select the 10-bit addressing format, write 1 to the expanded address enable (XA) bit of ICMDR and make sure the free data format mode is off (FDF = 0 in ICMDR).
Figure 13-12 I2C Module 10-bit Addressing
Format