SPRUJB6B November 2024 – May 2025 AM2612
The memory that holds the interrupt vector for each interrupt is protected by SECDED ECC. Single-bit errors are corrected and written back. Double-bit errors are not corrected. If a double-bit error occurs while trying to load a vector, then the MSS_VIM_DEDVEC register is used to provide the default vector for the coreN_IRQADDRV signal, the MSS_VIM_IRQVEC register, and the MSS_VIM_FIQVEC register. The MSS_VIM_DEDVEC should point to an ISR that handles the fact that there was an uncorrectable error in the interrupt handling.
Some possible remediating actions would be to:
It is up to the user and the application to determine the appropriate action.
An interrupt that has an uncorrectable vector error (and thus uses the DED vector) will still have the priority of the original interrupt (that is, for masking purposes). This makes it possible for a higher priority interrupt to supercede the handling of the error.
Control and reporting are done by the R5FSS ECC aggregator. When in lockstep mode, only the RAM for CPU0 is used.