SPRUJE7A January   2025  – July 2025 F29H850TU , F29H859TU-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Differences From C28x
    2. 1.2 Function Listing Format
  5. 2F29H85x Flash API Overview
    1. 2.1 Introduction
    2. 2.2 API Overview
    3. 2.3 Using API
      1. 2.3.1 Initialization Flow
        1. 2.3.1.1 After Device Power Up
        2. 2.3.1.2 On System Frequency Change
      2. 2.3.2 Building With the API
        1. 2.3.2.1 Object Library Files
        2. 2.3.2.2 Distribution Files
      3. 2.3.3 Key Facts for Flash API Usage
  6. 3API Functions
    1. 3.1 Initialization Functions
      1. 3.1.1 Fapi_initializeAPI()
    2. 3.2 Flash State Machine Functions
      1. 3.2.1  Fapi_setActiveFlashBank()
      2. 3.2.2  Fapi_setupBankSectorEnable()
      3. 3.2.3  Fapi_issueAsyncCommandWithAddress()
      4. 3.2.4  Fapi_issueBankEraseCommand()
      5. 3.2.5  Fapi_issueProgrammingCommand()
      6. 3.2.6  Fapi_issueAutoEcc512ProgrammingCommand()
      7. 3.2.7  Fapi_issueDataAndEcc512ProgrammingCommand()
      8. 3.2.8  Fapi_issueDataOnly512ProgrammingCommand()
      9. 3.2.9  Fapi_issueEccOnly64ProgrammingCommand()
      10. 3.2.10 Fapi_issueAsyncCommand()
      11. 3.2.11 Fapi_checkFsmForReady()
      12. 3.2.12 Fapi_getFsmStatus()
    3. 3.3 Read Functions
      1. 3.3.1 Fapi_doBlankCheck()
      2. 3.3.2 Fapi_doVerify()
      3. 3.3.3 Fapi_doVerifyByByte()
    4. 3.4 Informational Functions
      1. 3.4.1 Fapi_getLibraryInfo()
    5. 3.5 Utility Functions
      1. 3.5.1 Fapi_flushPipeline()
      2. 3.5.2 Fapi_calculateEcc()
      3. 3.5.3 Fapi_isAddressEcc()
      4. 3.5.4 Fapi_getUserConfiguration()
      5. 3.5.5 Fapi_setFlashCPUConfiguration()
      6. 3.5.6 Fapi_issueProgBankMode()
  7. 4SECCFG and BANKMGMT Programming Using the Flash API
    1. 4.1 BANKMGMT Programming
    2. 4.2 SECCFG Programming
  8. 5Allowed Programming Ranges for All Modes
  9. 6Recommended FSM Flows
    1. 6.1 New Devices From Factory
    2. 6.2 Recommended Erase Flow
    3. 6.3 Recommended Bank Erase Flow
    4. 6.4 Recommended Program Flow
  10. 7References
  11.   A Flash State Machine Commands
  12.   B Typedefs, Defines, Enumerations and Structure
    1.     B.1 Type Definitions
    2.     B.2 Defines
    3.     B.3 Enumerations
      1.      B.3.1 Fapi_FlashProgrammingCommandsType
      2.      B.3.2 Fapi_FlashBankType
      3.      B.3.3 Fapi_FlashStateCommandsType
      4.      B.3.4 Fapi_StatusType
      5.      B.3.5 Fapi_ApiProductionStatusType
      6.      B.3.6 Fapi_BankID
      7.      B.3.7 Fapi_FLCID
      8.      B.3.8 Fapi_BankMode
      9.      B.3.9 Fapi_CPU1BankSwap
      10.      B.3.10 Fapi_CPU3BankSwap
      11.      B.3.11 Fapi_FOTAStatus
      12.      B.3.12 Fapi_SECVALID
      13.      B.3.13 Fapi_BankMgmtAddress
    4.     B.4 Structures
      1.      B.4.1 Fapi_FlashStatusWordType
      2.      B.4.2 Fapi_LibraryInfoType
  13.   Revision History

Fapi_issueDataAndEcc512ProgrammingCommand()

Sets up the flash state machine registers for the 512-bit (64 bytes) programming with user provided flash data and ECC data and issues the programing command to valid Flash memory.

Synopsis

Fapi_StatusType Fapi_issueDataAndEcc512ProgrammingCommand(
                                    uint32_t *pu32StartAddress,
                                    uint8_t  *pu8DataBuffer,
                                    uint8_t  u8DataBufferSizeInWords,
                                    uint8_t  *pu8EccBuffer,
                                    uint8_t  u8EccBufferSizeInBytes,
                                    uint32_t u32UserFlashConfig,
                                    uint8_t  u8Iterator
                                    )

Parameters

pu32StartAddress [in] 1024-bit aligned flash address to program the provided data and ECC.
pu8DataBuffer [in] Pointer to the Data buffer address. Address of the Data buffer can be 1024-bit aligned.
u8DataBufferSizeInWords [in] Number of bytes in the Data buffer. Max Databuffer size in words can not exceed 64.
pu8EccBuffer [in] Pointer to the ECC buffer address
u8EccBufferSizeInBytes [in] Number of bytes in the ECC buffer. Max Eccbuffer size in words can not exceed 16.
u32UserFlashConfig [in] User flash configuration bitfield
u8Iterator [in] Iterator for program and erase operations on interleaved banks.
0: Data Flash/non-interleaved
1: B0 or B2 (dependent on provided address)
2: B1 or B3 (dependent on provided address)

Description

This function programs both the user provided 512-bit data (second parameter) and 8 bytes of ECC data (fourth parameter) together at the user provided 512-bit aligned flash address. The address of data provided must be aligned on a 512-bit memory boundary and the length of data must correlate to the supplied ECC. That means, if the data buffer length is 64 bytes, the ECC buffer must be 8 bytes (1 ECC bytes corresponding to 64-bit data).

Each byte of pu8EccBuffer corresponds to each 64-bit of the main array data provided in the pu8DataBuffer. For more details, see Table 3-6.

The Fapi_calculateEcc() function can be used to calculate ECC for a given 64-bit aligned address and the corresponding data.

For allowed programming range for the function, see Table 3-4.

Table 3-4 Permitted programming range for Fapi_issueDataAndEcc512ProgrammingCommand()
Flash API Main Array ECC BANKMGMT and SECCFG
Fapi_issueDataAndEcc512ProgrammingCommand() Allowed Allowed Not allowed

Restrictions

  • As described above, this function can program only a max of 512-bits (given the address provided is 512-bit aligned) at a time. If the user wants to program more than that, this function can be called in a loop to program 512-bits at a time.
  • The Main Array flash programming must be aligned to 512-bit address boundaries and 64 bytes can only be programmed once per write or erase cycle.
  • 512-bit address range starting with a BANKMGMT or SECCFG address will always be programmed using 128-bit Fapi_issueProgrammingCommand().

Return Value

  • Fapi_Status_Success (success)
  • Fapi_Status_FsmBusy (FSM busy)
  • Fapi_Error_AsyncIncorrectDataBufferLength (failure: Data buffer size specified is incorrect. Also, this error will be returned if Fapi_EccOnly mode is selected when programming to the BANKMGMT or SECCFG spaces.)
  • Fapi_Error_AsyncIncorrectEccBufferLength (failure: ECC buffer size specified is incorrect.)
  • Fapi_Error_AsyncDataEccBufferLengthMismatch (failure: Data buffer size either is not 64-bit aligned or data length crosses the 128-bit aligned memory boundary.)
  • Fapi_Error_FlashRegsNotWritable (failure: Flash register writes failed. The user can make sure that the API is executing from the correct CPU.)
  • Fapi_Error_FeatureNotAvailable (failure: User passed a mode that is not supported.)
  • Fapi_Error_InvalidAddress (failure: User provided an invalid address. For the valid address range, see the F29H85x and F29P58x Real-Time Microcontrollers Data Sheet.)

Sample Implementation

(For more information, see the flash programming example provided in the F29H85x SDK at “f29h85x-sdk > examples > driverlib > single_core > flash > flash_mode0_512_program”).