SPRUJF1C November 2024 – December 2025 AM2612
The AM261x LaunchPad supports a Fast Serial Interface peripheral by terminating the AM261x FSI RX and TX signals to a 10-pin header. The interface has two lines of data and a clock line for both the receive and transmit signals. The 10-pin header is connected to the 3.3V System voltage supply. The AM261x internal pinmux can be used to select between FSI signals and other functionality of the associated pins. A 2:1 mux selects between FSI and OSPI1 signals, and routes to the appriopriate hardware on the PCB.
Figure 2-26 LP-AM261 FSI
Interface| OSPI1_MUX_SEL | Output |
|---|---|
| 0 | OSPI1 Signals |
| 1 | FSI Signals |