SPRUJH3 April   2025 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280034 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037C , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039C , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049C , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Configuring the Boot Mode
    1. 2.1 Standalone Boot
      1. 2.1.1 Boot Mode Select Pins (BMSP)
      2. 2.1.2 Boot Definition Table (BOOTDEF)
      3. 2.1.3 Boot ROM OTP Configuration Registers
      4. 2.1.4 CPU2 Boot Flow
    2. 2.2 Emulation Boot
  6. 3Programming the Flash
    1. 3.1 Flash API
    2. 3.2 Flash Kernels
  7. 4Bootloading Code to Flash
    1. 4.1 C2000 Hex Utility
    2. 4.2 Common Boot Modes
      1. 4.2.1 Boot to Flash
      2. 4.2.2 SCI Boot
      3. 4.2.3 CAN Boot
      4. 4.2.4 CAN-FD Boot
      5. 4.2.5 USB Boot
  8. 5FAQ
    1. 5.1 Selecting the BMSP GPIOs with a Software-based Implementation
    2. 5.2 Running a Flash Kernel from the Flash Instead of the RAM
    3. 5.3 No Symbols Defined When Debugging Boot ROM
    4. 5.4 Writing Values in the OTP Using the On-Chip Flash Tool
    5. 5.5 Writing Values in the OTP Using the Flash API Plugin
  9. 6Summary
  10. 7References

Bootloading Code to Flash

At the beginning of device boot up, the device decides if firmware is programmed into the Flash that needs to be executed or if code needs to be loaded in using a ROM loader. This is determined by examining the BMSPs, either defined by the user in the OTP, the emulation registers, or following the factory default boot configuration.

However, if a bootloader is selected that loads code from an external host, the application image needs to formatted and delivered in a specific procedure to be successfully programed into the RAM. Flash kernels can then be applied to bridge the gap between the Flash and RAM by linking the flash APIs to enable the kernels to erase and program flash.

This section demonstrates how to program and/or execute an application onto Flash for the most common boot modes (Flash, SCI, CAN, CAN-FD, and USB) by walking through the entire flow, from device boot configuration to flash kernel execution.