SPRZ193T January 2003 – December 2023 SM320F2812 , SM320F2812-EP , SMJ320F2812 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1
Figure 3-1 provides an example of the TMS320F281x device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 3-1. Some prototype devices may have markings different from those illustrated. Figure 3-2 shows an example of device nomenclature.
| SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | COMMENTS |
|---|---|---|---|
| Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX only. |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMX only. |
| B | Indicates Revision B | 0x0002 | Internal |
| C | Indicates Revision C | 0x0003 | TMP/TMX/TMS |
| D | Indicates Revision D | 0x0003 | Internal |
| E | Indicates Revision E | 0x0005 | Production device (TMS) |
| F | Indicates Revision F | 0x0006 | Internal |
| G | Indicates Revision G | 0x0007 | Production device (TMS) |
Figure 3-2 Example of Device Nomenclature