| ADC |
ADC: Initial Conversion |
Yes |
Yes |
| ADC |
ADC: Temperature Sensor Minimum Sample Window
Requirement |
Yes |
Yes |
| ADC |
ADC: Offset Self-Recalibration Requirement |
Yes |
Yes |
| ADC |
ADC: ADC can Become Non-Responsive When ADCNONOVERLAP or RESET
is Written During a Conversion |
Yes |
Yes |
| Memory |
Memory: Prefetching Beyond Valid Memory |
Yes |
Yes |
| eCAN |
eCAN: Abort Acknowledge Bit Not Set |
Yes |
Yes |
| eCAN |
eCAN: Unexpected Cessation of Transmit Operation |
Yes |
Yes |
| GPIO |
GPIO: GPIO Qualification |
Yes |
Yes |
| GPIO |
GPIO: GPIO Pullup Enabled on Reset |
Yes |
Yes |
| Oscillator |
Zero-Pin Oscillator: Modification to Oscillator Frequency
Parameter |
Yes |
Yes |
| Watchdog |
Watchdog: Incorrect Operation of CPU Watchdog When WDCLK Source
is OSCCLKSRC2 |
Yes |
Yes |
| Oscillator |
Oscillator: CPU Clock Switching to INTOSC2 May Result in
Missing Clock Condition After Reset |
Yes |
Yes |
| eQEP |
eQEP: eQEP Inputs in GPIO Asynchronous Mode |
Yes |
Yes |
| eQEP |
eQEP: Position Counter Incorrectly Reset on Direction Change
During Index |
Yes |
Yes |
| ePWM |
ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the
End of the Blanking Window |
Yes |
Yes |
| ePWM |
ePWM: Trip Events Will Not be Filtered by the Blanking Window
for the First 3 Cycles After the Start of a Blanking
Window |
Yes |
Yes |