SPRZ455F December 2020 – February 2025 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
MCU: MCU domain may hang if main domain is issued a
reset
The MCU domain is designed to be able to work completely independently from the main domain of the device. If the main domain is put in to reset, the MCU domain should continue to function uninterrupted, even if there are pending transactions from MCU masters to Main domain slaves. The purpose of this feature is to ensure that if the main domain must be put in to reset because of a fault, the MCU domain continues to operate uninterrupted. The Main domain could subsequently be brought out of reset and re-started. The issue is that sometimes, if there is a transaction outstanding from MCU to Main domain and Main is put in to reset (unexpectedly or intentionally because of a fault) it may lead to a hang in the MCU domain interconnect. This can in turn cause MCU masters to become unresponsive.
The first workaround is to ensure that there are no MCU transactions outstanding from MCU to Main when Main is in reset. This must be enforced at the system level. It is possible to use this workaround when the Main domain reset is done in an orderly fashion, but may not be possible if the main domain reset is unexpected or driven by a fault.
The second workaround is to not put the Main domain in to reset in the case of a fault. The Main domain may be otherwise ‘taken off line’, but the system does not actually assert warm reset to the Main domain. In this case, the MCU will continue to function properly, including unwinding any pending transactions from the Main domain.
Neither of these workarounds is robust to an unexpected reset or a fault that requires reset to prevent propagation or damage.