SPRZ455F December   2020  – February 2025 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1

 

  1.   1
  2. 1Modules Affected
  3. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  4. 3Silicon Revision 2.0/1.1/1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 2.0/1.1/1.0 Usage Notes
      1.      i2134
      2.      i2453
    2. 3.2 Silicon Revision 2.0/1.1/1.0 Advisories
    3.     i2024
    4.     i2038
    5.     i2048
    6.     i2049
    7.     i2050
    8.     i2052
    9.     i2053
    10.     i2054
    11.     i2055
    12.     i2062
    13.     i2063
    14.     i2064
    15.     i2065
    16.     i2067
    17.     i2079
    18.     i2081
    19.     i2083
    20.     i2085
    21.     i2086
    22.     i2087
    23.     i2090
    24.     i2091
    25.     i2092
    26.     i2093
    27.     i2094
    28.     i2095
    29.     i2096
    30.     i2097
    31.     i2098
    32.     i2099
    33.     i2100
    34.     i2101
    35.     i2102
    36.     i2103
    37.     i2103
    38.     i2115
    39.     i2116
    40.     i2117
    41.     i2118
    42.     i2119
    43.     i2120
    44.     i2121
    45.     i2122
    46.     i2123
    47.     i2124
    48.     i2126
    49.     i2127
    50.     i2128
    51.     i2129
    52.     i2131
    53.     i2132
    54.     i2133
    55.     i2134
    56.     i2137
    57.     i2138
    58.     i2139
    59.     i2141
    60.     i2143
    61.     i2144
    62.     i2145
    63.     i2146
    64.     i2147
    65.     i2148
    66.     i2149
    67.     i2150
    68.     i2151
    69.     i2152
    70.     i2153
    71.     i2154
    72.     i2155
    73.     i2157
    74.     i2159
    75.     i2160
    76.     i2161
    77.     i2162
    78.     i2163
    79.     i2164
    80.     i2166
    81.     i2168
    82.     i2171
    83.     i2173
    84.     i2174
    85.     i2177
    86.     i2178
    87.     i2179
    88.     i2180
    89.     i2182
    90.     i2183
    91.     i2184
    92.     i2185
    93.     i2187
    94.     i2188
    95.     i2189
    96.     i2190
    97.     i2191
    98.     i2196
    99.     i2197
    100.     i2198
    101.     i2199
    102.     i2200
    103.     i2205
    104.     i2207
    105.     i2208
    106.     i2210
    107.     i2211
    108.     i2213
    109.     i2214
    110.     i2215
    111.     i2216
    112.     i2217
    113.     i2219
    114.     i2221
    115.     i2227
    116.     i2228
    117.     i2229
    118.     i2230
    119.     i2232
    120.     i2233
    121.     i2234
    122.     i2235
    123.     i2238
    124.     i2239
    125.     i2244
    126.     i2245
    127.     i2246
    128.     i2249
    129.     i2253
    130.     i2257
    131.     i2271
    132.     i2274
    133.     i2275
    134.     i2277
    135.     i2278
    136.     i2279
    137.     i2283
    138.     i2305
    139.     i2306
    140.     i2307
    141.     i2310
    142.     i2311
    143.     i2312
    144.     i2320
    145.     i2329
    146.     i2351
    147.     i2362
    148.     i2366
    149.     i2371
    150.     i2383
    151.     i2399
    152.     i2401
    153.     i2409
    154.     i2414
    155.     i2418
    156.     i2422
    157.     i2424
    158.     i2435
    159.     i2454
  5.   Trademarks
  6.   Revision History

Modules Affected

Table 1-1 shows the module(s) that are affected by each usage note.

Table 1-1 Usage Note by Modules
MODULEUSAGE NOTE
C7x i2453 — C7x: LBIST MISR changed on SR2.0
USBi2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation

Table 1-2 shows the module(s) that are affected by each advisory.

Table 1-2 Advisories by Modules
MODULE ADVISORY SILICON REVISIONS AFFECTED
SR 1.0 SR 1.1 SR 2.0
AASRC i2229 — AASRC: AASRC is not supported YES YES YES
ADC i2151 — ADC: Debounce time control register NO YES YES
Boot i2038 — Boot: FAT16 Fails When Root Block Resides in More Than One Cluster YES YES YES
i2081 — Boot: ROM Maximum Timeout per Boot Mode Will Be Half of the Original Value from TRM YES NO NO
i2307 — Boot: ROM does not properly select OSPI clocking modes based on BOOTMODE YES YES YES
i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation NO YES YES
i2371 — Boot: ROM code may hang in UART boot mode during data transfer YES YES YES
i2414 — Boot: Ethernet PHY Scan and Bring-Up Flow doesn't work with PHYs that don't support Auto Negotiation YES YES YES
i2418 — Boot: Secure ROM Panic due to Certificate Info not present YES YES YES
i2422 — Boot: ROM timeout for MMCSD filesystem boot too long YES YES YES
i2435 — Boot: ROM timeout for eMMC boot too long YES YES YES
C66x i2214 — C66x: Writes to different endpoints can land out of order if not fenced YES YES YES
C71x i2063 — C71x: VCOP Aliasing for CPU Loads and Stores Is Not Supported for Non-Aligned Accesses to the Last Line in the IBUF Buffers YES YES YES
i2064 — C71x: DMA Accesses to L1D SRAM May Stall Indefinitely in the Presence Cache Mode Change or Global Writeback in Specific Conditions YES YES YES
i2065 — C71x: The C71x Memory System and CPU May Stall Indefinitely in the Presence L1D Snoops YES YES YES
i2079 — C71x: DMA Accesses to L1D SRAM May Stall Indefinitely in the Presence of CPU Traffic in Specific Conditions YES YES YES
i2087 — C71x: MMA HWA_STATUS Reports Errors Before Application Starts YES YES YES
i2117 — C71x: Register Corruption When MMA HWARCV is in Parallel With Load or Store With uTLB Miss YES NO NO
i2131 — C71x: Memory System May Hang During L2 Writeback Invalidate Operation when L2 Scrubber is Enabled YES YES YES
i2199 — C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary YES YES YES
i2213 — C7x SE: SE Can Hang when a 2 dataphase transaction comes back with differing rstatuses YES YES YES
i2219 — C7x SE: SE Returning incorrect rstatus for uTLB faults YES YES YES
i2271 — C7x SE: SE Can Hang on Page Fault/UMC Error Occurring During SEBRK YES YES YES
i2399 — C7x: CPU NLC Module Not Clearing State on Interrupt YES YES YES
i2454 — C7x: Reset forcing not allowed YES YES NO
CBASS i2207 — CBASS: Command Arbitration Blocking YES YES YES
i2235 — CBASS Null Error Interrupt Not Masked By Enable Register YES YES YES
CC i2221 — CC: Invasive and Non-Invasive debug enable settings are reset by MCU_RESETz YES YES YES
CP i2283 — Restrictions on how CP Tracer Debug Probes can be used YES YES YES
CPTS i2083 — CPTS: GENF (and ESTF) Reconfiguration Issue YES YES YES
i2141 — CPTS: GENF and ESTF Nudge Value Not Cleared by Hardware YES YES YES
CPSW i2139 — CPSW: ALE Incorrectly Routes Packets With CRC Errors YES YES YES
i2148 — CPSW: CPSW Directed Frames are Not Observed When Classification Overrides the Destination Port Via the Egress Opcode Feature YES YES YES
i2184 — CPSW: IET express traffic policing issue YES YES YES
i2185 — CPSW: Policer color marking issue YES YES YES
i2208 — CPSW: ALE IET Express Packet Drops YES YES YES
i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES YES YES
CPSW9G i2179 — CPSW9G: Reset isolation not working correctly YES NO NO
CSI i2052 — CSI: CSI-Rx to CSI-Tx Retransmit Path Is Unavailable YES YES YES
i2190 — CSI: CSI_RX_IF may enter unknown state following an incomplete frame YES YES YES
DDR i2155 — DDR: Controller DDRSS_CTL_194[9-8] BIST_RESULT Status is Unreliable YES YES YES
i2157 — DDR: Controller Anomaly in Setting Wakeup Time for Low Power States YES YES YES
i2159 — DDR: VRCG High Current Mode Must be Used During LPDDR4 CBT YES YES YES
i2160 — DDR: Valid VRef Range Must be Defined During LPDDR4 Command Bus Training YES YES YES
i2166 — DDR: Entry and exit to/from Deep Sleep low-power state can cause PHY internal clock misalignment YES YES YES
i2182 — DDR: Dual-rank non-power-of-2 density not supported with row-cs-bank-col address mapping YES YES YES
i2232 — DDR: Controller postpones more than allowed refreshes after frequency change YES YES YES
i2244 — DDR: Valid stop value must be defined for write DQ VREF training YES YES YES
i2274 — DDR: Including DDR in BSCAN causes current alarm on the DDR supply YES YES YES
DMADVR i2233 — DMADVR: Link/link_safer sync issue between MAIN and MCU YES YES YES
DMSC i2245 — DMSC: Firewall Region requires specific configuration YES YES YES
i2275 — DMSC Secure Boot ROM: Potential Secure Boot vulnerability with explicit EC curve parameters in X.509 certificate YES YES YES
DPHY i2174 — DPHY: Reset sequence issue can lead to undefined module behavior YES NO NO
DRU i2198 — DRU, UTC: Issue with setting ICNT3 to 0 when not being used YES YES YES
i2215 — DRU: TR Submission can be corrupted by C7x writes coming out of order if Non-Atomic TR Submission Mechanism is Used YES YES YES
DSS i2097 — DSS: Disabling a Layer Connected to Overlay May Result in Synclost During the Next Frame YES YES YES
ECC_AGGR i2049 — ECC_AGGR: Potential IP Clockstop/Reset Sequence Hang due to Pending ECC Aggregator Interrupts YES YES YES
i2191 — ECC_AGGR: Erroneous non-correctable parity error assertion for RAM80 YES NO NO
eMMC i2144 — eMMC: VIO Supply Sequencing YES YES YES
FSS i2048 — FSS: MCU_FSS0_WRT_TYPE Register is Logging Incorrectly YES YES YES
GIC i2101 — GIC: ITS Misbehavior YES YES YES
HyperBus i2119 — HyperBus: HyperBus is Not Functional YES NO NO
I3C i2150 — I3C: SDAPULLEN drives low instead of Hi-Z YES YES YES
i2197 — I3C: Slave mode is not supported YES YES YES
i2205 — I3C: Command fetched during pending IBI is not properly processed in some cases YES YES YES
i2216 — I3C: Command execution may fail during slave-initiated IBI address byte reception YES YES YES
IA i2196 — IA: Potential deadlock scenarios in IA YES YES YES
Internal Diagnostics Modules i2103 — Internal Diagnostics Modules: Incorrect Reporting of ECC_GRP, ECC_BIT and ECC_TYPE Information for Functional Safety Errors YES YES YES
ICSSG i2230 — ICSSG: ICSSG is not supported YES YES YES
i2305 — ICSSG: PRU RAM WRT during active FDB lookup write data corruption YES YES YES
JTAG i2228 — JTAG: TAP used by Debuggers may be inaccessible if TRSTn device pin is never asserted YES YES YES
MCAN i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID YES YES YES
i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID YES YES YES
MCU i2173 — MCU domain may hang if main domain is issued a reset YES NO NO
i2217 — Recommended POST selection via MCU_BOOTMODE[09:08] YES YES NO
MDIO i2329 — MDIO: MDIO interface corruption (CPSW and PRU-ICSS) YES YES YES
MMCSD i2024 — MMCSD: Peripherals Do Not Support HS400 YES YES YES
i2090 — MMCSD: MMCSD1 and MMCSD2 Speed Issue YES NO NO
i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small YES YES YES
MSMC i2116 — MSMC: Set-hazarding logic withholding RT access waiting on NRT access completion YES YES YES
i2149 — MSMC: MSMC Scrubber Only Targets Bottom 16 of 32 Ways of SRAM/L3$ YES YES YES
i2187 — MSMC: Cache Resize to 0 Refreshes Tags instead of Updating them YES YES YES
OSPI i2115 — OSPI: OSPI Boot Doesn't Support Some xSPI Modes or xSPI Devices YES NO NO
i2189 — OSPI: Controller PHY Tuning Algorithm YES YES YES
i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable YES YES YES
i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash YES YES YES
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode YES YES YES
PCIe i2085 — PCIe: Gen2 Capable Endpoint Devices Always Enumerate as Gen1 YES YES YES
i2086 — PCIe: MMA Unsupported Request (UR) or Configuration Request Retry Status (CRS) in Configuration Completion Response Packets Results in External Abort YES YES YES
i2094 — PCIe: End of Interrupt (EOI) Not Enabled for PCIe Legacy Interrupts YES YES YES
i2100 — PCIe: Endpoint Destination Select Attribute (ASEL) Based Routing Issue YES YES YES
i2147 — PCIe: Incorrect translation completion type sent by RP for ATS translation request YES YES YES
i2152 — PCIe: Lock up may occur if link down event happens during non-posted command YES YES YES
i2153 — PCIe: Incorrect Reserved Bit Handling in TS1 Packet YES YES YES
i2154 — PCIE: Lane deskew failure during L0s exit YES YES YES
i2183 — PCIe: Link up failure when unused lanes are not assigned to PCIe Controller YES YES YES
i2238 — PCIe: The 2-L SerDes PCIe Reference Clock Output can exceed the 5.0 GT/s Data Rate RMS jitter limit YES YES YES
i2239PCIe: The 2-L SerDes PCIe Reference Clock Output is temporarily disabled while changing Data Rates — YES YES YES
i2246 — PCIe: Automatic compliance entry fails when unused SERDES lanes are not assigned to PCIe Controller YES YES YES
PLL i2178 — PLL: Corrupted writes to CAL_IN field of PLL12_CAL_CTRL register YES YES YES
i2424 — PLL Programming Sequence May Introduce PLL Instability YES YES YES
POK i2277 — POK: De-Glitch (filter) is based upon only two samples YES YES NO
PRG i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure YES YES YES
PRU-ICSSG i2180 — PRU-ICSSG: FDB table corruption during switch operation YES NO NO
PSIL i2137 — PSIL: Clock stop operation can result in undefined behavior YES YES YES
i2138 — PSIL: Configuration accesses and source thread teardowns may cause data corruption YES YES YES
R5FSS i2099 — R5FSS: Deadlock Might Occur When One or More MPU Regions is Configured for Write Allocate Mode YES YES YES
i2118 — R5FSS: Debug Access in Lock-Step Mode May Result in Failure YES YES YES
i2129 — R5FSS: High Priority Interrupt is Missed by VIM YES YES YES
i2132 — R5FSS: Interrupt Preemption (Nesting) is Unavailable if Using VIM Vector Interface for Interrupt Handling YES YES YES
i2133 — R5FSS: Lock-Step Mode of Operation is Not Functional YES NO NO
i2161 — Debugger Cannot Access VIM Module While It Is Active YES YES YES
i2162 — R5FSS: The Same Interrupt Cannot be Nested Back-2-Back Within Another Interrupt YES YES YES
i2164 — R5FSS: Errors in ECC injection logic are not detected because the pending interrupts are tied low YES YES YES
i2210 — R5FSS : ATB Flush requests are suppressed YES YES
i2227 — R5FSS: Error interrupt CCM_COMPARE_STAT_PULSE_INTR incorrectly driven YES YES YES
RA i2054 — RA: Reads from GCFG Region Can Cause Spurious RAM ECC Errors YES YES YES
i2095 — RA: Peek to Tail Returns Wrong Data YES YES YES
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set YES YES YES
Reset i2200 — RESET: TIMEOUT_PER does not work when programmed to 0 value. YES YES YES
RINGACC i2177 — RINGACC: The ring accelerator’s debug transaction trace stream can be corrupted by certain ring access sequences YES YES YES
ROM Code i2306 — ROM Code: Need to turn off internal termination resistors in SERDES YES YES YES
SA2_UL i2098 — SA2_UL: Auth/Decrypt Operations with 2nd Input Thread Does Not Send the DMA Packet Out YES YES YES
2-L SerDes i2171 — 2-L SerDes: State Change Monitor interrupts are not available YES YES YES
SGMII i2362 — SGMII: Marvell PHY does not ignore the preamble byte resulting in link failure YES YES YES
STOG i2121 — STOG: Flushing Gasket while there is a write transaction in flight can result in dropped write responses YES NO NO
i2122 — STOG: Flushing Gasket concurrently with Gasket receiving a write response can cause indefinite non-idleness YES YES YES
i2123 — STOG: Timed Out Emulation Debug write responses from the Slave Gasket always return Success YES YES YES
i2124 — STOG: Read command timeout can result in a gasket hang YES NO NO
i2126 — STOG: Error miscounting when there are two concurrent timeouts or two concurrent unexpected responses YES YES YES
i2127 — STOG: SRC side write data bus hang when a write command timeout occurs the same cycle as last acceptance on DST side YES YES YES
UART i2096 — UART: Spurious UART Interrupts When Using DMA YES YES YES
UDMAP i2055 — UDMAP: Packet Mode Descriptor Address Space Select Field Restrictions YES YES YES
i2143 — UDMAP: TX Channel SA2UL teardown issue YES YES YES
i2146 — UDMA: Force teardown bitfield readback is masked in realtime TX/RX registers YES YES YES
i2163 — UDMAP: UDMA transfers with ICNTs and/or src/dst addr NOT aligned to 64B fail when used in "event trigger" mode YES YES YES
i2168 — UDMAP: Spurious ECC errors due to MAIN/MCU NAVSS rofifo_wr_byten issue YES YES YES
i2320 — UDMA, UDMAP: Descriptors and TRs required to be returned unfragmented YES YES YES
i2234 — UDMA: TR15 hangs if ICNT0 is less than 64 bytes YES YES YES
UFS i2102 — UFS: Auto-Hibernate can cause false entry/exit errors YES YES YES
i2211 — UFS: Hibernate Exit can result in link reinitialization YES YES YES
USART i2310 — USART: Erroneous clear/trigger of timeout interrupt YES YES YES
i2311 — USART: Spurious DMA Interrupts YES YES YES
USB i2050 — USB: Endpoint OUT Data Queue is Locked Up Due to a Data Packet for an Endpoint that Does Not Have Associated TRB YES YES YES
i2067 — USB: Race Condition while Reading TRB from System Memory in Device Mode YES YES YES
i2091 — USB: 2.0 PHY Hangs if Received Signal Amplitude Crosses Squelch Threshold Mmultiple Times Within the Same Packet YES YES YES
i2092 — USB: Invalid Termination of DMA Transfer for Endpoint Following Isochronous Endpoint in SuperSpeed Device Mode YES YES YES
i2093 — USB: DMA Hangs if USB Reset is Received During DMA Transfer in Device Mode YES YES YES
i2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation YES YES YES
i2409 — USB: USB2 PHY locks up due to short suspend YES YES YES
VPAC i2188 — VPAC, DMPAC: UTC ECC writeback on queue memory can cause TR corruption YES YES YES
VTM i2053 — VTM: Software Reads from On-Die Temperature Sensors Can Be Corrupted YES YES YES
i2128 — VTM: VTM Temperature Monitors (TEMPSENSORs) Should Use a Software Trimming Method YES YES YES
i2145 — VTM: Enabled interrupt event status registers incorrectly return raw unmasked values YES YES YES
xSPI i2257 — xSPI boot mode redundant image boot failure NO YES YES