SPRZ506B October 2022 – December 2023 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Flash: Single-Bit ECC Error Interrupt is Not Generated
0, A, B, C
If the single-bit ECC error threshold is configured as 0, the single-bit error interrupt is not generated when there is a single-bit error.
Set the error threshold bit field (FLASH_ECC_REGS ERR_THRESHOLD.ERR_THRESHOLD field) to a value greater than or equal to 1. Note that the default value of the threshold bit field is 0.