SPRZ578A December   2024  – July 2025 AM2752-Q1 , AM2754-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  4. 2Silicon Revision Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2284
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2120
      4.      i2137
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2249
      9.      i2253
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2377
      16.      i2383
      17.      i2401
      18.      i2427
      19.      i2431
      20.      i2435
      21.      i2436
      22.      i2438
      23.      i2449
      24.      i2455
  5. 3Trademarks
  6. 4Revision History

i2377

RAT input signals rbytecnt and wbytecnt calculation is wrong

Details:

RAT logic inside R5SS uses rbytecnt and wbytecnt to determine if read or write access crosses the region boundaries configured by SW. The rbytecnt and wbytecnt values sent to the RAT are computed in the R5SS, but the equations used are incorrect.

This results in the RAT not detecting or erroneously detecting region boundary crossings.

Workaround(s):

Because the Cortex-R5 AXI main interface transactions do not cross a 32 byte boundary, there are no issues with region boundaries equal to or greater than 32 bytes. The issue only occurs when the region boundary is less than 32 bytes. Therefore software can not set region boundaries that are less than 32 bytes.