SSZTCX6A April   2023  – February 2025 TPS7H5001-SP , TPS7H5002-SP , TPS7H5003-SP , TPS7H5004-SP , TPS7H5005-SEP , TPS7H5006-SEP , TPS7H5007-SEP , TPS7H5008-SEP , TPS7H6003-SP , TPS7H6005-SEP , TPS7H6005-SP , TPS7H6013-SP , TPS7H6015-SEP , TPS7H6015-SP , TPS7H6023-SP , TPS7H6025-SEP , TPS7H6025-SP

 

  1.   1
  2.   2
    1.     3
    2.     Conclusion
    3.     Additional resources
    4.     Trademarks

Kurt Eckles

In the satellite industry, dramatic increases in local data processing, support for higher throughput communication links and the rapid adoption of electrical propulsion systems are driving demand for much higher performance electrical power systems (EPSs). The EPS is part of the bus section of a satellite, providing structural support and housing subsystems such as power, thermal management, communication and propulsion. The EPS generates, stores, regulates and distributes power to all other subsystems and payloads onboard the satellite.

The unique challenges and constraints of space missions require optimizing size, weight and power (SWaP). Here are some of the reasons why SWaP is such a big deal in satellite designs:

  • Mission requirements: Ever increasing requirements such as data transmission rate, resolution and sensitivity can impact a satellite’s SWaP requirements.
  • Launch limitations: Satellites have size constraints, weight constraints and cost-of-launch constraints that can be $1,000s to $10,000s per kilogram based on the intended orbit.
  • Power generation: Satellites generally rely on solar panels, and the size and weight of the panels limit the amount of generated power. The power-generation capacity also affects the weight and size of components, like batteries, and functions such as power distribution and thermal management.
  • Operational efficiency: SWaP optimization enables satellites to operate more efficiently in space, resulting in better performance and longer mission lifetimes.

Because power is one of the most valuable resources on a satellite, maximizing EPS efficiency can help extend mission lifetimes, reduce mass and volume, and minimize thermal management overhead.

Beyond efficiency, an EPS must also handle a wide range of voltages and currents because of the number of power-supply topologies. Figure 1 shows some of the most common topologies.

 Common power-supply topologies in satellite power architecturesFigure 1 Common power-supply topologies in satellite power architectures

The components and functions, shown in Figure 2, of a typical satellite EPS are:

  • Solar panels (or energy generation): Solar panels are the primary power source for most satellites.
  • A battery (or energy storage): The battery stores excess power generated by the solar panels during daylight hours, and provides power to the satellite during an eclipse or when the solar panels are not generating enough power.
  • Power-conditioning unit (PCU): The PCU regulates the electrical output of the solar panels and battery to provide a stable and consistent voltage and current to the rest of the satellite.
  • Power-distribution unit (PDU): The PDU distributes power generated by the solar panels and battery to the various subsystems and payloads onboard the satellite.
  • Backup power supply: If the primary EPS fails, a backup power supply will help maintain the most essential functions until the restoration of the primary system.
 A typical satellite EPSFigure 2 A typical satellite EPS

Designers can solve their SWaP design challenges in satellite systems by combining pulse-width modulation (PWM) controllers with gate drivers and either silicon MOSFETs or GaN FETs. This approach enables development of optimized power supplies for the different parts of the EPS system.

When developing EPS, designers can select from a diverse range of the voltage and current level radiation-hardened Half-bridge GaN FET gate drivers that scale across the satellite’s entire EPS power tree. Available devices include the TPS7H6003-SP (200V), TPS7H6013-SP (60V), TPS7H6023-SP (22V) (100 krad TID, 75 MeV⋅cm2/mg SEL immune) and radiation-tolerant TPS7H6005-SEP (200V), TPS7H6015-SEP (60V), TPS7H6025-SEP (22V) (50 krad TID, 43 MeV⋅cm2/mg SEL immune). These gate drivers provide design flexibility by supporting a number of different power supply topologies and input formats.

Additionally, designers can also use PWM controllers like radiation-hardened TPS7H5001-SP and radiation-tolerant TPS7H5005-SEP PWM controllers that are designed to support a range of different power-supply implementations.

TI developed the following reference designs to help engineers working with space-grade PWM controllers and GaN FET gate drivers in various power-supply circuits, not only in the EPS, but also on select payload applications:

  • Non-isolated high-voltage buck design
    • Features a 300W non-isolated synchronous buck topology that supports an input of 50V to 150V with an output of 28YV, using the above mentioned PWM controllers and gate drivers.
    • This design is optimized for regulating the highly variable output of 100-V solar panels before the satellite passes the power to the battery storage portion of an EPS subsystem.
    • Example TI reference kit: PMP23552
  • Isolated full-bridge design
  • Non-isolated high-current multiphase buck design
    • This design uses PWM controller and gate drivers in a multiphase synchronous buck topology to support an input of 11V to 14V with an output of 0.8 V and again uses GaN FETs in the power stage. The design is dual-phase implementation that is capable of supporting 80A while maintaining acceptable DC and AC tolerance.
    • Designers can extend designs to more phases, helping meet design requirements like high current (100A+) and low input voltages (sub-0.8 V) needed to power the core rails of some advanced field-programmable gate arrays, ASICs or multicore processors.
    • Example TI reference kit: TIDA-010958
    • Additional resources: Application note "12 VIN to 1 VOUT Single Phase Buck Converter Using TPS7H5001-SP Controller."

Conclusion

With power being one of the most valuable resources on a satellite, the EPS architecture can have a significant impact on the overall design. TI’s radiation-validated PWM controller families provide high efficiency and support a wide range of topologies, as well as an architecture that’s deployable in a diverse set of missions and orbits.

Trademarks

All trademarks are the property of their respective owners.